(0)| 6/25/2009 9:52 AM | |
|
Joined: 9/27/2006 Last visit: 1/20/2026 Posts: 12481 Rating:
|
Hello SergMRC; First, have a look at the following attachment, it is an extract from the Protool Communications manual (Teil 1), for protool 5.0. But it should help you understand the concepts. The manual showshow you can connect a MP270B with a CPU943, either using serial (AS511) connection or Profibus-DP. It will show you the details of the connection, area pointers, data types, and most points to consider in such an application. Come back with more specific questions when you need them clarified. Hope this helps, Daniel Chartier AttachmentCommProtool_S5.pdf (609 Downloads) |
| 6/25/2009 10:06 AM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Hello, Perhaps this FAQ can helps:How does time synchronization work between S5 and a Windows-based operator panel? Regards Hristo Mihalev |
| 6/25/2009 1:06 PM | |
|
Posts: 3 Rating:
|
Hello, I interest the file of the project *.pdb for MP270B key. Shall very grateful You for this. Many thanks!!! |
Follow us on