(1)| 7/31/2024 1:48 PM | |
|
Joined: 6/10/2008 Last visit: 12/1/2025 Posts: 198 Rating:
|
Hello, I have TIA v17 project that has PLC Tags as an empty table. On the other hand there is a table with HMI tags. I want to sync these two, but what ever option I choose, PLC tags are still empty. It seems that Sync works to sync HMI tags from PLC tags and not vice versa. I also have these variables in DBs, so I wonder how to create PLC tags from HMI tags and if that's not possible then how to create PLC tags from DB variables. Attached is xlsx export from HMI tags. There is a column "PLC tags", but actually in PLC Tags in hierarchy, under Show all tags, I get an empty table. Thank you AttachmentHMITags.xlsx (342 Downloads) |
Last edited by: Jasner at: 07/31/2024 13:50:35 |
|
Follow us on