9/13/2024 1:09 PM | |
Joined: 9/26/2010 Last visit: 9/13/2024 Posts: 1 Rating:
|
I have a SINAMICS CU310-2 PN drive and as per the requirement of the on going project I had to update drive firmware from 4.6 to 4.8. I'm sure that firmware update was done accurately but after this update Ready (RDY) LED blinked at 0.5Hz frequency. I tried all possible solutions but it did not changed. So again I downgraded firmware from 4.8 to 4.6. Now LED is ON continuously but X127 port does not respond for communication. I tried parameter settings and all the IP related settings. Still problem is here. Plz help me to solve this. The project is urgent. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 09/16/2024 09:17:52New subject after splitting |
|
Follow us on