(0)| 5/4/2023 7:18 PM | |
|
Posts: 5 Rating:
|
Hello, I'm trying to commision a sinumerik one system (NCU 1740, ver. 6.15). I've gotten to the point of trying to download the PLC program. I can compile with no errors on the software or hardware. When I try to actually set the PLC to RUN, it immediately runs into an error. SINUMERIK message: DB access error: DB1000 Explanation: An error occurred during access to the data blocks, the data block cannot be used. See alarm: 404007 Then: Temporary CPU error: User programmed STOP request in FB 25003 affecting OB 1 execution I have not been able to find any reference to alarm 404007, or errors related to FB25003(LBP_InternalProc7) or DB1000(LBP_CtrlEnergy) AttachmentDiagnostics.txt (659 Downloads) |
| 5/9/2023 7:25 AM | |
|
Joined: 7/12/2021 Last visit: 1/15/2024 Posts: 26 Rating:
|
Is the toolbox in your project actually and also loaded to the PLC? |
| 5/9/2023 1:13 PM | |
|
Posts: 5 Rating:
|
Yes it is |
| 9/19/2024 11:31 AM | |
|
Joined: 3/9/2022 Last visit: 12/16/2025 Posts: 1 Rating:
|
May you can share how you solved this problem? |
Follow us on