10/11/2022 1:06 PM | |
Joined: 8/18/2022 Last visit: 1/24/2023 Posts: 29 Rating:
|
Hello guys, You helped me a lot and I continue learning PLC. I am trying to build my electrical diagram and I am a little bit confused. What is the "24 VDC sensor out" input used for? Is it just to power my sensors? Thank you! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/12/2022 03:59:31New subject after splitting |
|
10/12/2022 12:58 PM | |
Joined: 7/7/2010 Last visit: 9/12/2025 Posts: 16094 Rating:
|
The best use for the 24VDC Sensor Output is for accepting digital inputs aux contacts from relays and contactors. Attempting to power even a couple prox switches can exceed the available current capacity of the 24VDC Sensor Output supply -read last part from @qwazee's prior post above. I tend to not wire that to anything - except for what has been suggested, AC powered S7-1200's to sense aux contact dig inputs. It also works well for switches (without a light). Basically, if it is a dry contact, it can be a good solution if it saves installing a separate 24VDC supply. That's a rather rare exception for most projects, but if it's a small desktop prototyping project where you have a starter kit AC powered s7-1200, it's great for powering the dig input simulator switches.
|
science guy |
|
This contribution was helpful to
1 thankful Users |
Follow us on