12/16/2016 1:56 PM | |
Joined: 11/24/2016 Last visit: 1/16/2025 Posts: 19 Rating:
|
Hello ,it is not possible to me to create a stanalone project on pcs 7 V8.1 .All times when i try to do it the messages bellow appears -The OS object (1) could not be created under WINCC -The OS object (2) could not be created under WINCC -An error has occurred in the creation of a technological hierarchy AttachmentPCS7_Problem.docx (230 Downloads) |
12/16/2016 3:52 PM | |
Joined: 3/14/2008 Last visit: 9/16/2025 Posts: 2216 Rating:
|
Did you compress the PCS7 project folder by instance? See: Link Do you have the correct authorization. If the logged on user is part of Simatic HMI group? Did you change the default location of your PCS7 projects? If so, you have to run program: "SimaticRights.exe" which can be found on the DVD. Otherwise a reinstall of AS-OS engineering is probably a solution. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on