10/9/2024 2:40 PM | |
Joined: 8/16/2010 Last visit: 6/18/2025 Posts: 640 Rating:
|
Hello all. Also had the same issue. We have active sensor which have pins for 24vdc power supply, input for SP+ and SP- (4-20mA), and output for feedback FB+ and FB- (4-20mA). How to connect active sensor to this type of card 6ES7134-6HD00-0BA1? Also have analog output card 6ES7135-6HD00-0BA1. First solution: To use the card 6ES7134-6GD01-0BA1. Second solution: Is there any transducer which can accept active signal from sensor and convert it to passive... Maybe one Turck IMS-AI-UNI/24VDC, for SP set to 0-10V (from AO card) -> 4..20mA (to sensor) and one for FB set to 4-20mA (from sensor) -> 0..10V (to AI card) I'm not sure if conversion from AO card is needed... BR ------------------------------------------------------------------------------------------ |
Last edited by: Milosh at: 10/09/2024 14:57:04Last edited by: Moderator_Lan at: 10/11/2024 07:35:37New subject after splitting |
|
10/12/2024 3:46 PM | |
Joined: 3/28/2010 Last visit: 9/18/2025 Posts: 1173 Rating:
|
Yes, there are isolator/signal conditioners that can convert an active 4-20mA signal (on the input) to a passive, loop powered signal (on the output). I suspect Phoenix Contact, Weidmuller, and Turck have active-to-passive isolators, but I can't quote a part number. |
Follow us on