(0)| 10/23/2023 3:24 PM | |
|
Posts: 2 Rating:
|
Hello everyone, I'm trying to establish communication with an EthernetIP device but I'm failing to configure it. I'm receiving the status code 7002 but I nevere achieve the isActive bool to be set to true (so no communication is being done). Here I attach the EDS file and some screenshots of my configuration. If someone can check them to ensure I'm not doing anything wrong it would be very helpfull. TIA Portal v18 is being used. If more information is required let me know! :) Cheers, Albert AttachmentethIP_help.zip (717 Downloads) |
Last edited by: albertarla at: 10/23/2023 15:25:52 |
|
| 10/24/2023 1:32 PM | |
|
Posts: 2 Rating:
|
The status 16#7002 means that it's all ok and the block is working. Nevertheless the isAtive bit is false so no communication is being done. I think the problem I'm facing is in the configuration. but not sure why or where is the problem. I was expecting to receive ethernetIP messages (so the isActive would be true and there would be data written to the output db). I attached the eds file I'm using which is needed to configure properly the block and the configuration I set. I need help to find the configuration problem or why I'm not communicating properly. I used this: link as tutorial to configure the block. I have checked the HW and everything looks right. |
Last edited by: albertarla at: 10/24/2023 13:33:35Last edited by: Jen_Moderator at: 10/25/2023 07:33:51Link optimized. |
|
| 10/15/2024 4:11 PM | |
|
Joined: 3/12/2020 Last visit: 10/15/2024 Posts: 11 Rating:
|
albertarla: Did you manage to solve this? I'm struggling with the exact same scenario (S71500 with an EtherNet/IP adapter). The only thing I'm missing is the 'Active' bit. |
|
Aguaribay |
|
Follow us on