10/19/2024 6:31 PM | |
Joined: 12/18/2014 Last visit: 9/10/2025 Posts: 35942 Rating:
|
What do you consider to be daytime? What times exactly do you mean by that? |
10/20/2024 7:52 AM | |
Joined: 6/18/2021 Last visit: 10/23/2024 Posts: 32 Rating:
|
Dear Sir, Please find the attached program file. There are a total of 8 units, with 7 running and 1 on standby. Requirements: - All units should change over daily based on the weekly timer block at 10:00 AM. - All units should run 24 hours a day. - Require weakly timer block programming as On/off Timing, weak selection as per attached program Best regards, Paigambar Momin
Attachment7 running, 1 standby.zip (276 Downloads) |
Last edited by: Momin paigambar at: 10/20/2024 07:55:08 |
|
10/20/2024 10:47 AM | |
Joined: 6/11/2019 Last visit: 9/7/2025 Posts: 2628 Rating:
|
Hello Momin, Unfortunately, your two descriptions are not very clear. They also contradict each other in some ways. As I understand it, however, the system switches to a different unit every day at 10:00 a.m. If the current unit is faulty or inactive, it should switch to the standby unit. If my assumption is correct, my modification of your program will definitely help you. Greetings Ella_68 Attachment7 running , 1 stanby weakly timer program (mod 1).zip (305 Downloads) |
Last edited by: Ella_68 at: 10/20/2024 11:03:12 |
|
Follow us on