10/22/2024 3:52 PM | |
Joined: 7/22/2023 Last visit: 4/30/2025 Posts: 7 Rating:
|
Hello, We have a S7 300 CPU with 7 ET200S stations. All of them are getting recognized but 2 stations. I have done the following checking, 1) Changed the connectors 2) Changed the cable 3) Replaced the ET200S which I am confident with but only these 2 stations are just not visible. I have 24V supply to all the PM E modules in the rack. The error in the hardware config shows Module not available. PFA photo and file. Thanks in advance. AttachmentPDFen.pdf (284 Downloads) |
Follow us on