10/17/2024 8:38 AM | |
Joined: 11/29/2021 Last visit: 9/3/2025 Posts: 1 Rating:
|
Hi all, Currently I am running PCS7 and one of my OS server was faulty. So I intend to replace to the new IPC and CP card which is 1623. I also plan to run my OS server virtualy in the new IPC later. Question: 1) If I change the CP card, how the PLC able to communicate since the MAC address is not same. My faulty IPC using Cp1613. Can I change the MAC address for new CP later? Im using ISO connection for PLC communication. I not intend to change the original MAC configured in project file. 2) Do I need to use hypervisor instead the normal/commercial vmware? No other way to let the virtualized OS server to communicate with the new CP1623? Thanks all. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 10/17/2024 08:50:27New subject after splitting |
|
Follow us on