(0)| 11/5/2024 12:26 PM | |
|
Joined: 7/2/2024 Last visit: 9/4/2025 Posts: 3 Rating:
|
Hey there. i am trying to work on this same. I tried to write the parameter p2599 using 1500 plc but then i was using wrrec block. And it did not work. Can you explain me how did you write parameters using sina_pos block. if i use mode 5 in sina_pos block, then the actual position is becoming 0. But then what should i do if i have to write a value 100 to the actual position using the same block? Much appreciated. Thanks and regards Athish ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 11/05/2024 12:34:24New subject after splitting |
|
| 11/6/2024 4:45 PM | |
|
Joined: 10/11/2006 Last visit: 1/20/2026 Posts: 6051 Rating:
|
Hello, use "Absolute Encoder Adjustment function block "EncoderAdjustment"" https://support.industry.siemens.com/cs/ww/en/view/109760317 |
|
With best regards, |
|
| 11/7/2024 11:00 AM | |
|
Joined: 7/2/2024 Last visit: 9/4/2025 Posts: 3 Rating:
|
Thanks a lot. Will take a look into that and see how it works. |
Follow us on