11/11/2024 9:38 AM | |
Joined: 3/14/2008 Last visit: 9/11/2025 Posts: 2216 Rating:
|
Hi, There are two types of licenses for the CPU410-5H. AS RT PO:
AS PO:
According to your description, you likely have the AS RT PO. |
If I could help you, you can use the RATE button. Thank you. |
|
11/11/2024 3:28 PM | |
Joined: 1/17/2022 Last visit: 8/19/2025 Posts: 3 Rating:
|
I have the two types of license, but i have problem at transfer the licenses to CPU. I'm following the steps, according to Siemens procedure (https://support.industry.siemens.com/cs/ww/de/view/96839331) When i try transfer the licenses to CPU (step 5, page 71), the error happens. My question is whether this license is the correct one, or whether it should be an "upgrade" license instead of a "single". ty Attachmenterror license PO.zip (98 Downloads) |
Last edited by: Moderator_Lan at: 11/11/2024 15:30:27link optimized |
|
11/11/2024 3:42 PM | |
Joined: 1/17/2022 Last visit: 8/19/2025 Posts: 3 Rating:
|
Hi there. Can you help me about this topic below? Ty |
11/11/2024 3:47 PM | |
Joined: 3/14/2008 Last visit: 9/11/2025 Posts: 2216 Rating:
|
Hi, I'm a little confused, one of the screenshots shows OS RT PO, that is a license that should be located in ALM on the OS server. The other one is AS RT PO which is a license that should remain on the engineering station in ALM. No need to transfer it to the CPU, that is only in case of AS PO which are transferred to the SEC. In order to transfer a license to the SEC, you need a release and activation file after connecting the CPU410 to ALM. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on