11/20/2024 9:34 AM | |
Joined: 7/11/2024 Last visit: 9/9/2025 Posts: 200 Rating:
|
Hi EhsanNiknami13701123 Have you configured the right Power Supply in TIA Portal? Error LED blinking may be due to mismatched hardware configuration (Status LEDs) Have you tried restarting the PLC and the power supply? Is your PC's IP address in the same subnet as the PLC's IP address? Have you temporarily disabled the firewall or antivirus to check if they are blocking the connection? |
Last edited by: JimHalpert at: 11/20/2024 09:35:45If this post has been useful, don't forget to rate it!😊 |
|
11/20/2024 9:39 AM | |
Joined: 7/19/2022 Last visit: 9/11/2025 Posts: 436 Rating:
|
Hello EhsanNiknami13701123, Do you have PG/PC interface correctly configured? You have to select on the S7ONLINE (STEP 7) -> "Network card of the PC".TCPIP.1 |
Last edited by: JBS98 at: 11/20/2024 09:40:37If this Information really helps, you could use the Rate function |
|
Follow us on