(0)| 11/25/2024 3:42 PM | |
|
Joined: 10/15/2024 Last visit: 11/27/2025 Posts: 2 Rating:
|
Hi everyone. I need help with the html code for the S7-1500 web server. My goal is to change the background color of the lights on a web page based on an input variable (0 or 1) read from the PLC. In the attachment I have the code, the variables are defined here, but I have a problem with the logic in the "script" part, where I try to change the background color based on the input values. I think the problem will be in accessing variables in the script section. Could someone help me with this problem? Reading variables and listing them works fine for me. The text file with the html code is in the attached txt file AttachmentDotaz.txt (268 Downloads) |
Follow us on