11/26/2024 11:03 AM | |
Joined: 3/14/2008 Last visit: 9/8/2025 Posts: 2216 Rating:
|
Hi, Safety Matrix does not create the technological blocks (VlvL etc.), but rather involves the input and output tags by creating F driver blocks/function blocks and those signals are used in the safety matrix. The Safety Matrix blocks are added to the existing CFC program. See the following manual starting page 81 chapter 7: Link Since a recent update for PCS7 V9.0 (I believe), Safety blocks are also supported by CMT (Control Module Types). |
Last edited by: Oreca at: 11/26/2024 11:08:12If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
1 thankful Users |
Follow us on