(0)| 10/3/2023 9:54 AM | |
|
Joined: 2/5/2013 Last visit: 1/19/2026 Posts: 345 Rating:
|
Dears Sirs, any one that experimented the https://weinzierl.de/en/products/knx-ip-baos-777/ ? Many year have passed, I've seen siemens got TP/IP interfaces but in the application example use an external PROFINET/KNX gateway:
In this example too much devices are involved data import/export, this is no good solution. I want the simplest way to manage an existing KNX system via an S7-1200. To manage my logic via PLC. How could it be possibile that via a simple TP/IP interface a raspberry pi can control a KNX plant and a Siemens PLC could not Any advice is appreciated. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/13/2023 10:14:22New subject after splitting |
|
| 10/13/2023 12:00 PM | |
|
Joined: 4/28/2015 Last visit: 11/27/2025 Posts: 10970 Rating:
|
Hello,
but any S7 controller with ETH interface and OUC capable also does |
Last edited by: Duris_I at: 10/13/2023 12:01:57Last edited by: Duris_I at: 10/13/2023 12:03:26Last edited by: Duris_I at: 10/13/2023 15:58:18With best regards... |
|
| 11/26/2024 7:16 PM | |
|
Joined: 11/27/2015 Last visit: 12/5/2025 Posts: 2 Rating:
|
I'm using this KNX Modbus TCP Gateway. Modbus TCP communication is default available in a S7-1200 and S7-1500 controller |
This contribution was helpful to
|
|
| 12/5/2025 9:21 AM | |
|
Joined: 11/27/2015 Last visit: 12/5/2025 Posts: 2 Rating:
|
Also S7KNXcom is a good solution. Downside is that this software is only working on a 1500 and not on a 1200 CPU because of the Multicast implementation. Having this running for over a year now. Very stable. |
Last edited by: TechMo at: 12/05/2025 09:23:50 |
|
This contribution was helpful to
|
|
Follow us on