11/27/2024 7:11 PM | |
Joined: 8/19/2012 Last visit: 7/4/2025 Posts: 129 Rating:
|
dear All Due to some errors made by operators, I want to add a confirmation message when clicking on Run (Are you sure) with Yes or No, and when clicking Yes, the operation process is completed, or clicking No cancels the completion of the process. I have an attached attempt. note: i used PCS7 V9.0 SP3 with CEMAT LIBRARY Type Mineral. best regard AttachmentC_DRIVE.docx (104 Downloads) |
Follow us on