(0)| 11/28/2024 3:28 PM | |
|
Joined: 5/27/2023 Last visit: 7/14/2025 Posts: 20 Rating:
|
Hello everybody, I have a question for you all. I have to integrate a Siemens S7-1200 PLC with a ABB IRB1200 robot via PROFINET. I did the following setup but it seems that the signals doesn't change when testing. I'll attach a document explaining the steps and the setup that I did with some pictures to illustrate. If needed, I can send the two GSD files mentioned in it. I hope you can help me solve the problem. Thank you for all your time and help! Best regards, Claudiu Muresan AttachmentPLC-Robot Profinet communication setup.pdf (266 Downloads) |
Last edited by: Claudiu Muresan at: 11/28/2024 15:30:05 |
|
Follow us on