(0)| 11/6/2024 1:56 PM | |
|
Joined: 4/6/2022 Last visit: 10/24/2025 Posts: 9 Rating:
|
Hi to everyone, I hope you are well. I have the necessity to comunicate my Siemens S7-410 5H (PCS7 V9.1) with a controller ABB AC800M trought is Profinet Communication module CI871 that works as a Master. Can I used PN/PN Coupler A5E39544711-AH to stablish this communication? ABB Control System AC800M has not Profinet Slave Module and we need to do that only with Profinet. |
| 12/2/2024 12:29 PM | |
|
Joined: 2/24/2011 Last visit: 1/21/2026 Posts: 100 Rating:
|
Hi, yes, it's possible. The released nodules with PCS 7 9.1 SP2 are documented in point 8 of the "SIMATIC PCS 7 V9.1 SP2 Software Updates". Please note the application samples: and It is valid for SIMATIC PCS 7 V9.1.You need the GSDML file of the PN/PN coupler for the configuration at ABB side. |
This contribution was helpful to
|
|
Follow us on