12/2/2024 8:27 PM | |
Joined: 9/29/2020 Last visit: 12/3/2024 Posts: 1 Rating:
|
Hi, I was wondering if someone could clarify something for me. Does the Operator Action List truly contain just actions which are generated by the control room operators actions? That is to say, via a mouse click or a keyboard action at the client screen. Or can an entry into this list be generated by logic running in the background? Like a button which has a feed input to turn it on or off without any operator intervention? I ask because we are seeing actions appear in the Operators Action List which were not generated by the operator. In the past, this has been a means of "monitoring" what has happened that either should, or should not have been done by an individual. So there really needs to be some clarification as to how this works. Thanks! ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 12/03/2024 07:33:19New subject after splitting |
|
Follow us on