12/10/2024 3:24 PM | |
Joined: 7/11/2024 Last visit: 8/4/2025 Posts: 200 Rating:
|
Hello berruezaVW To integrate 5K NTC temperature sensors (PT5000) with the S7-1200, you can use the SM 1231 RTD module (6ES7534-7QE00-0AB0)It is compatible with resistance sensors, so is suitable for NTC thermistors. Also, this module allows individual configuration of each channel, so you can chose different scaling parameters for different temperature probes You can check the datsheet of this module here: 6ES7534-7QE00-0AB0 I hope you find it useful! PS: for next time write your posts in English😉 |
If this post has been useful, don't forget to rate it!😊 |
|
This contribution was helpful to
1 thankful Users |
Follow us on