(2)| 1/12/2024 9:18 AM | |
|
Joined: 9/23/2005 Last visit: 1/21/2026 Posts: 4450 Rating:
|
Hi As from TIA V19, it is possible to use the Visual Studio Code as a platform to edit WinCC Unified Scripts in a more comfortable way, with the help of JS Connector. General sequence:
TIPs:
Sample project (archived from TIA Portal as .zap19 and after that compacted in .zip format to be uploaded here) user= User, all password = Password1! Attachmentvisual.zip (734 Downloads) |
Last edited by: Denilson Pegaia at: 01/12/2024 09:23:52Last edited by: Denilson Pegaia at: 01/12/2024 09:26:02Last edited by: Denilson Pegaia at: 01/12/2024 09:27:18Last edited by: Denilson Pegaia at: 09/13/2024 11:26:20. Denilson Pegaia |
|
This contribution was helpful to
|
|
| 6/11/2024 12:12 PM | |
|
Joined: 9/23/2005 Last visit: 1/21/2026 Posts: 4450 Rating:
|
Hi, as V19 up2 it is also possible to debug Scripts in Visual Studio. The Visual studio extension (and the installation manual) are available at SIMATIC WinCC Unified RT Debugger TIP:
|
|
Denilson Pegaia |
|
| 12/18/2024 1:20 PM | |
|
Joined: 9/15/2022 Last visit: 1/16/2026 Posts: 18 Rating:
|
I had the same problem, apparently due to a certificate in the JS Connector 1.3.0 that has expired at the end of Oct/2024 or something. I installed the latest JS Connector for V20 (yes, even if using Tia V19) and it now plays ok. Hope this helps. |
| 12/11/2025 10:21 AM | |
|
Joined: 9/23/2005 Last visit: 1/21/2026 Posts: 4450 Rating:
|
The JS Connector, manual and cast are also available for V21 in https://support.industry.siemens.com/cs/br/en/view/109825899 |
|
Denilson Pegaia |
|
Follow us on