1/7/2025 8:15 AM | |
Joined: 5/17/2011 Last visit: 9/11/2025 Posts: 35 Rating:
|
To be more specific: The term acquire would be wrong for CMTs. It is always linked to exactly one EMT/EPHT via block contacts. Acquire only applies to EMT/EMT or EPHT/EMT combinations. It uses some kind of arbitration logic (or multiplexer) called MARC. The attached picture should clarify the difference between both approaches (see chapter 10.5.5 of compendium C, sadly also in the english documents the text in the picture are German). As documentation I recommend to read the Compendium C. If you have access to the Intranet/Extranet (for example as Siemens partner) I especially recommend this document: Engineering and automation of batch processes with PCS 7 along ISA-88 models Depending on your needs there are also other options to share a CMT, like ShrdResS from the APL. |
Last edited by: Trivial at: 01/07/2025 08:17:01 |
|
This contribution was helpful to
1 thankful Users |
1/7/2025 12:20 PM | |
Joined: 5/17/2011 Last visit: 9/11/2025 Posts: 35 Rating:
|
I've been asking myself the same question. Maybe something is in preparation? I really don't know, sadly. |
Follow us on