1/9/2025 6:35 PM | |
Joined: 3/14/2008 Last visit: 9/8/2025 Posts: 2216 Rating:
|
Hi, It is not possible to add more then one technological condition in a transition. I sent in a SR three years ago to make that possible. The downside of technological transitions is that there is a small non scalable windo where all the transitions are listed. You can use AND/OR and also nest them. It can get unreadable very quickly especially if you use NOT's in the logic. For one of our customers we now use a combination of technological and "regular" conditions. This will make it somewhat better to read for the operators. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
2 thankful Users |
Follow us on