12/18/2024 3:52 PM | |
Joined: 12/18/2024 Last visit: 1/20/2025 Posts: 4 Rating:
|
Dear Nulizhang and others, Recently we’ve bought a used Gildemeister NEF 320 lathe. This lathe is powered/controlled by a Simodrive 611 with 2 LT modules (rebranded by Heidenhain) One of these LT modules controls the main spindle motor, it has a lot of numbers on it: SIMODRIVE LT-MODULE INT.50A (Heidenhain calls it DDC2) 1P 6SN1123-1AA00-0CA1 S TT-566018901015 VERSION A This LT module has 2 large IGBT modules (EUPEC BSM50GX120DN2(6)) On both of these units the N terminal has burned away (see pictures) My Questions are: What might have caused this problem? Is it a common problem? Strangely, the machine was still operating perfectly, it was a pure coincidence that we discovered the burned PCB. I can buy new IGBT units but these are expensive and to replace them is a lot of work. On the other hand, replacement boards are readily available on the internet but there are differences in version numbers. The outside cover of the unit is marked VERSION A, the PCB itself has a name and number box that says: SIEMENS ABCDE with ABCD crossed out and E encircled (more or less) which seems to indicate a version E for the PCB, the number is 462018-7925.11 What do these version letters mean? There is a complete unit available on the internet but this is a VERSION C (outside label) Do I need to get the exact same version letters? Is there a chance that the problem will reoccur once I have replaced the unit? All in all my questions boil down to: what should I do to solve this problem? Thanks a lot for your time and effort and I hope you can help us out. Sincerely, Jaap. Attachmentphotos.pdf (304 Downloads) |
1/13/2025 11:23 AM | |
Joined: 12/18/2024 Last visit: 1/20/2025 Posts: 4 Rating:
|
Very disappointing (i'm sorry to say this) |
Follow us on