(0)| 1/28/2025 10:40 AM | |
|
Joined: 3/12/2024 Last visit: 1/30/2026 Posts: 234 Rating:
|
Hi, please try the following steps: Skip eMMC Boot The firmware update might have reset the boot order, prioritizing the eMMC, which is currently empty. To bypass the eMMC and force the device to boot from an external medium (µSD or USB):
Use UART to Modify Boot Order If skipping the eMMC does not resolve the issue, you can use a UART connection to manually change the boot order:
If none of these steps will fix your issue we can try to reflash a compatible firmware image. BR |
Follow us on