(1)| 1/28/2025 8:33 AM | |
|
Joined: 3/12/2024 Last visit: 1/21/2026 Posts: 232 Rating:
|
Hi smyh_mahmoodi154, for the first commissioning of your IOT2050 with IndOS I would recommend you to use a Display Port monitor or an active HDMI-DP adapter or an UART cable for a serial connection (we always use this cable). On the first boot you should see the so-called mel-setup after some seconds: This setup will guide you through the necessary configuration steps of the IndOS. The IndOS on IOT2050 does not come with a static IP address by default (unlike the Example Image) so a connection via PuTTY SSH is not possible by default -> use one of the options mentioned above. For detailed information I highly recommend you our forum entry How to setup IndOS on IOT2050 Advanced with the additional PDF. There are all steps mentioned you need to know for first commissioning. Regarding your 2nd request IndOS vs Example Image: The choice between using the pre-installed Industrial OS or the SD card-based Example Image depends on your use case: Pre-installed Industrial OS
Example Image on SD Card:
BR |
This contribution was helpful to
|
|
| 1/28/2025 7:23 PM | |
|
Joined: 12/14/2024 Last visit: 9/5/2025 Posts: 4 Rating:
|
Thank you so much for your clarification! |
Follow us on