1/30/2025 6:43 PM | |
Joined: 12/1/2024 Last visit: 7/9/2025 Posts: 5 Rating:
|
I hope the second image is more convincing! |
1/31/2025 5:28 PM | |
Joined: 12/1/2024 Last visit: 7/9/2025 Posts: 5 Rating:
|
You are right! Sorry! I have attached the program...Attachmentheating.zip (167 Downloads) |
1/31/2025 10:43 PM | |
Joined: 6/11/2019 Last visit: 9/14/2025 Posts: 2630 Rating:
|
I would replace B005 with an RS element. Then you have the option of additionally triggering the heating of the 500l tank on the negative edge of B016 when the target temperature of the 200l tank is reached. Regards Ella_68 Attachmentheating mod1.zip (181 Downloads) |
2/2/2025 11:16 AM | |
Joined: 6/11/2019 Last visit: 9/14/2025 Posts: 2630 Rating:
|
Hi AutoGen,
If I haven't made any mistakes, the program in the appendix should correspond to your description. The block B005 sets the priority. Regards Ella_68 Attachmentheating mod2.zip (190 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on