(0)| 2/11/2025 12:32 PM | |
|
Joined: 8/3/2009 Last visit: 1/16/2026 Posts: 16644 Rating:
|
Hello SebastianHansenSU... Check the Information in the manual: https://support.industry.siemens.com/cs/ww/en/view/109977691/184332071691 We would need also more information for troubleshooting like used IT Adresses for Networkadapters, and Virtual PLC Sim Network adapter, is the network adapter connected to the Virtual PLC Sim Advanced switch? Settings in the PLC Sim Advanced, and also Which PLC type do you want to simulate (with FW Version) in which TIA Version. Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on