2/12/2025 9:36 AM | |
Joined: 8/3/2009 Last visit: 9/17/2025 Posts: 16447 Rating:
|
Hello AutoGen_8350221 this will not work because the GetText is a VBA function and cannot be used in VBS! The easiest way would be to use a Textref Tag to dynamise the text property: give the Textref Tag as startvalue the ID of the textlibrary entry you need. Or you can also check if the ODK function still works from this older FAQ: https://support.industry.siemens.com/cs/de/en/view/29420392 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on