2/19/2025 6:49 AM | |
Joined: 1/21/2013 Last visit: 9/9/2025 Posts: 4099 Rating:
|
Hi Thenameinforum, An ODBC driver for Microsoft SQL Server is installed on the WinCC Unified Comfort panel. To access an SQL Server via ODBC, a corresponding driver must be installed on the client. No additional installation is required on the server. This means that your current databases are not affected by the installation. However, providing access to another client may allow the client - your Unified Panel - to modify the data in the database, which can of course lead to possible data loss. Kind regards |
This contribution was helpful to
2 thankful Users |
Follow us on