2/18/2025 9:57 PM | |
Joined: 11/26/2024 Last visit: 2/18/2025 Posts: 1 Rating:
|
Hello cordial greetings! I'm in need of help, when simulating Wincc Unified from incorrect version installed error. I have already uninstalled all versions and installed only the v19 version and still keep. I am enclosing an image of the errors. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 02/19/2025 09:04:58New subject after splitting |
|
2/19/2025 12:43 PM | |
Joined: 7/10/2024 Last visit: 8/22/2025 Posts: 180 Rating:
|
Hello! This issue arises because, following the installation of WinCC Unified ES, the simulation must be downloaded and installed independently. - SIMATIC WinCC Unified PC Runtime V19 Simulation & Trial |
If you found this post helpul, I'd greatly appreciate your feedback with the rate function |
|
2/20/2025 10:49 AM | |
Joined: 8/3/2009 Last visit: 9/12/2025 Posts: 16409 Rating:
|
Hello AutoGen_4204116 Yes, also for simulation you have to install the Unifeied PCRT Software , its not inlcuded in the main TIA Portal DVD. Also check with this FAQ if you have set up everythiing correcly after installation not to run into other issues: https://support.industry.siemens.com/cs/de/en/view/109806850 Good luck Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on