(0)| 2/25/2025 9:40 AM | |
|
Joined: 8/3/2009 Last visit: 1/16/2026 Posts: 16644 Rating:
|
Hello RoxanaMorar So I think S71200 is OPC UA Server (because it can not act as OPC UA Client) and the WInCC Runtime Advanced is OPC UA Client? Do you have checked this FAQ: https://support.industry.siemens.com/cs/ww/en/view/63481236 There are examples for each side. Check also in the rejected folders of the RT Advanced Client certificate folders if there is a rejected PLC certificate (dometimes you have to trust also if you do not use security) Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on