5/22/2024 9:42 AM | |
Joined: 3/11/2019 Last visit: 9/1/2025 Posts: 1653 Rating:
|
Hi, even if Windows in a VM is used, in addition to that the Apple silicon M* CPUs are ARM based which is an additional issue in combination with TIA. There is a big thread in this forum, some people managed to get TIA working on an M1. The thread is not to M3 specifically, but maybe useful anyways. Tia Portal on new Apple M1 chipBut even this somehow will work, TIA is still used on an not supported OS with a not supported ARM CPU and most likely with a not supported VM. So there will be no support. And as TIA most likely will be used in an productive environment this is an additional risk if something doesnt work as intended. regards sancruz |
Feedback appreciated, please rate |
|
This contribution was helpful to
1 thankful Users |
Follow us on