(0)| 3/4/2025 6:50 PM | |
|
Joined: 9/21/2012 Last visit: 1/17/2026 Posts: 4851 Rating:
|
Is there a HMI connection between your PLC and HMI? How are the HMI tags connection configured? |
| 3/5/2025 9:52 AM | |
|
Joined: 3/4/2025 Last visit: 7/3/2025 Posts: 3 Rating:
|
The HMI is connected with an ethernet cable, and the HMI Tags are coded to be the same as the PLC ones |
| 3/5/2025 10:58 AM | |
|
Joined: 8/3/2009 Last visit: 1/16/2026 Posts: 16644 Rating:
|
Hello CasualStudent5391 which FW Version do you use in the PLC? Which Image Version is installed on the HMI? check if you hae set the korrect date/time on both systems Check also the basics in TIA regarding the connection: https://support.industry.siemens.com/cs/de/en/view/89852595 Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
| 11/12/2025 11:31 PM | |
|
Joined: 11/12/2024 Last visit: 12/23/2025 Posts: 1 Rating:
|
Hello, I have the same issue, how did you solve it? |
Follow us on