2/27/2015 7:59 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating:
|
Hello Brenton88, the question is, do you have Clients with own projects (Multi-Clients) or Clients without own projects, which have to access the project on the Server ? In the case of Multi-Clients, this Start-order is not relevant. In the case of the Clients without own projects, the Server has to be startet first, before the Clients. You can delay the Autostart on the Clients (and maybe on the second Server) according the description in the FAQ https://support.industry.siemens.com/cs/ww/en/view/19249315 But pay attention for the following FAQ too, it is relevant for the Servers. https://support.industry.siemens.com/cs/ww/en/view/23061262 Regards Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
Follow us on