3/10/2025 4:38 PM | |
Joined: 1/21/2013 Last visit: 9/12/2025 Posts: 4108 Rating:
|
Hi SpeedsterJuss, It would be easier to answer if you had provided more information, especially the current category 'STEP 7 (TIA Portal)' is not helpful as nothing sounds like a STEP 7 problem. Anyway, today I became aware of a similar problem that a colleague reported to development via a service request. In his project, a certain screen of his WinCC Unified Panel caused the TIA Portal V20 to crash. I was a bit surprised because I was using the same project without any crash, but I wanted to tell him that a SVG graphic within the screen contained invalid tags. But in the end this graphic was the reason for the crash and the crash did not happen to me because I configured my TIA Portal to use the Unified Screen Editor (Next Gen.). So if you are also using a WinCC Unified device, changing the editor may prevent the TIA Portal from crashing and allow you to find out which graphics are used in the screens. Or you can take a closer look at your graphics in the V17 version. Kind regards |
This contribution was helpful to
1 thankful Users |
Follow us on