3/7/2025 1:44 PM | |
Joined: 2/1/2010 Last visit: 9/15/2025 Posts: 213 Rating:
|
If you want it to default to the archive tags and not have to hit the button each time, append ";1" to the end of the TrendPictureName attribute in the Trends section of your block icons. example: "@pg_apl_trendMonAnL.pdl" becomes "@pg_apl_trendMonAnL.pdl;1" Do it in the library to apply it to your whole project for all block icons (you have to edit each one). If you have some tags that don't have tag logging turned on though, be advised that this will make you have to switch back on online view for it to work. So you may need to customize your block icons 1 by 1. |
If my post helped you, please rate. Thanks. |
|
This contribution was helpful to
1 thankful Users |
3/11/2025 1:01 PM | |
Joined: 2/1/2010 Last visit: 9/15/2025 Posts: 213 Rating:
|
Make the edits described earlier to each block icon on the @PCS7TypicalsV9...pdl or create alternate copies of the block icons you use and store them in a @PCS7Tyicalsv9custom...pdl (or whatever you want to call it) and save them with new names. e.g. MonAnL/1 > MonAnL/1h (1h = 1 with history trend) If you just change all the standard ones then you rerun block icon generation for your project and they all update. If you make copies so you can have both sets, then change all the block icon instances in CFC to the corresponding new block icon names and rerun block icon generation. The best time to do this change is at the beginning of the project but it's not always the case. Keep in mind after a version update you have to remake these template edits to ensure all new functionalities of block icons are intact. |
If my post helped you, please rate. Thanks. |
|
This contribution was helpful to
1 thankful Users |
Follow us on