(0)| 1/21/2025 1:06 PM | |
|
Joined: 4/9/2024 Last visit: 12/4/2025 Posts: 3 Rating:
|
Did you solve the problem? I have exactly the same message in engineering mode.. Please let me know if there is an answer! |
| 2/28/2025 10:38 AM | |
|
Joined: 11/5/2024 Last visit: 1/21/2026 Posts: 1 Rating:
|
DId you figure out a solution to this? |
| 3/12/2025 4:55 AM | |
|
Joined: 4/28/2015 Last visit: 11/10/2025 Posts: 3 Rating:
|
"Object.hasOwn is not a function" If you get this error in ABT Site, most likely the Microsoft component "WebView2" is not installed or outdated. This component is normally installed with Microsoft Edge browser. For normal Windows installation, it is updated via standard Windows updater and therefore (and for security reasons) it is mandatory to make sure, the PC has frequently internet connection and Windows update is performed. For Windows Server installation, it can be that this component is not automatically updated by Windows updater. The latest WebView2 component can be downloaded anyway via the official Microsoft Homepage or user this link (Evergreen Bootsrapper) : |
This contribution was helpful to
|
|
Follow us on