3/11/2025 8:55 AM | |
Joined: 7/10/2024 Last visit: 8/22/2025 Posts: 180 Rating:
|
Hello! The reference you have shared is part of the IPC 477C family. For this IPC the successor is the IPC477E. Please see the product announcement for this device: - https://support.industry.siemens.com/cs/ww/en/view/109744316 From the following link you are able to download the IPC configurator. With this configurator you are able to configure the IPC with the respective needed and available hardware. - SPC My main suggestion is through your business contact to help you in this migration, since IPC477D is involved. In case you don't have it, the following link may be useful for you. - Contact Database - Siemens AG I hope this comments help 🍀 |
If you found this post helpul, I'd greatly appreciate your feedback with the rate function |
|
This contribution was helpful to
1 thankful Users |
3/13/2025 11:24 AM | |
Joined: 8/3/2009 Last visit: 9/12/2025 Posts: 16409 Rating:
|
Hello BasemF You will need basically only another PanelPC for successor. So you would be able to use any of the available PanelPCs: https://mall.industry.siemens.com/mall/en/b1/Catalog/Products/10007484?tree=CatalogTree# You only have to care about size, OS (compatibility to your Software) and the Interfaces the PanelPCs offers. So you are not limited to the 477 family Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on