3/13/2025 12:44 PM | |
Joined: 6/23/2015 Last visit: 4/23/2025 Posts: 2 Rating:
|
Hello Experts i have a question in relation to that topic i have the CPU CPU 1516F-3 PN/DP the maximum number of I/o is related to the port x1 if i have more than the allowed number of profinet I/O devices (256) can i add a CM card "6GK7 542-1AX10-0XE0" to split the network and with that exceed the number of I/Os and will that affect the Performance of the CPU ? is it better to upgrade the CPU to 1517F version and then i have 512 ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 03/13/2025 12:56:00New subject after splitting |
|
Follow us on