3/14/2025 6:32 PM | |
Joined: 11/18/2021 Last visit: 6/3/2025 Posts: 1 Rating:
|
Hey everyone, I recently started working with it and wanted to integrate it to another project but I have not been able to make the firewall work on Windows 11, there is simply no communication between VLAN2 and VLAN1 even after defining IP rules. I use the following documentation for guidance in getting acquainted with the device (Industrial Security mit SIMATIC S7-1500). A few points worth mentioning: - Following the documentation, the experiment works perfectly on Windows 10 but not 11 (I am able to use firewall rules to establish communication between the VLANs for windows 10) - The firmware on the S615 is V07.02 (I tried with V08 as well) - I also tried using NETMAP and creating routes but it still didn't work - Using the Ping function within the S615 User interface, I am able to Ping the Conveyor belt in VLAN1 whilst the PC is connect to VLAN2 for both windows 10 and 11. Did anyone run into a similar problem and has some advice on how I can solve this problem? |
Last edited by: flipflop03 at: 03/16/2025 19:25:46 |
|
Follow us on