2/18/2025 12:20 PM | |
Joined: 12/6/2022 Last visit: 8/22/2025 Posts: 9 Rating:
|
Hi, can you explain more about the certificates? During the installation of WinCC Unified, I created the new certificate but it doesn't appear in the certificate manager. I have the same problem simulating the runtime, even I have the newest version installed with same update. Thank you, Domagoj ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 02/19/2025 08:14:15New subject after splitting |
|
2/19/2025 1:54 PM | |
Joined: 8/3/2009 Last visit: 9/11/2025 Posts: 16400 Rating:
|
Hello MarijanovicD you should first create a CA in the Unified Certificate Manager and then install the certificates (and export and install the CA) then do a restart of the Computer. Then open the Unified configuration and select the new Webserver certificate from your CA and run through the configurator. Then it should work: https://support.industry.siemens.com/cs/de/en/view/109806850 Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
3/15/2025 3:48 PM | |
Joined: 12/6/2022 Last visit: 8/22/2025 Posts: 9 Rating:
|
The solution was to install WinCC Unified Runtime PC V19. https://support.industry.siemens.com/cs/cy/en/view/109820988 With the same certificates, there is no General error in the Simatic Runtime Manager, and Simulation goes directly to the load screen, not the extended download to the device screen. Bye, Domagoj |
Last edited by: MarijanovicD at: 03/15/2025 15:50:15Last edited by: MarijanovicD at: 03/15/2025 15:51:18Last edited by: Moderator_Lan at: 03/17/2025 09:40:29link optimized |
|
Follow us on