9/20/2021 8:23 AM | |
Joined: 9/23/2015 Last visit: 1/25/2025 Posts: 13 Rating:
|
In TIA Portal v15.1 Update 5 (and lower versions) you can create an HMI project where you connect to a PLC still made in Step 7 v5.6. For this, you can use a "Device Proxy". But now I have a project on my desk where the "device proxy" is configured as a CPU317-F2 while it is actually a CPU315-F2. The device proxy is wrong. Probably they had a 315-F2 on the office, configured it with that. Went onsite and installed a 315-F2. Only one HMI connection is there for the operators communication. My problem: I have to create new tags, bu Does anyone know a solution except "delete" and "relinking everything"? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/19/2021 13:51:06New subject after splitting |
|
9/20/2021 8:24 AM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
create a new device proxy for the new plc type |
10/19/2021 1:03 PM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
see solution in the post above |
3/19/2025 7:14 AM | |
Joined: 5/3/2009 Last visit: 6/27/2025 Posts: 12 Rating:
|
In device view, try this |
Follow us on