(0)| 3/12/2025 8:58 PM | |
|
Joined: 10/17/2024 Last visit: 8/12/2025 Posts: 2 Rating:
|
Is it possible to use the IO2050 the other way around, as an end-device to communicate with a gateway? This question is because I have a mobile device that I want to connect to my local network and, in this case, the iot2050 would be a data centralizer that would do some simple calculations before sending this data via lorawan to, perhaps, another iot2050 acting as a gateway. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 03/12/2025 23:31:40New subject after splitting |
|
| 3/21/2025 1:25 PM | |
|
Joined: 3/12/2024 Last visit: 1/20/2026 Posts: 232 Rating:
|
Hello! From technical perspective this should be possible. Typically the IOT2050 is used as the gateway to forward and process data but to use it as an end-device to send data you need to have the following points in mind:
I also recommend you a look into our LoRaWAN gateway application example. BR |
Follow us on