5/3/2010 2:55 PM | |
Joined: 3/14/2008 Last visit: 9/8/2025 Posts: 2216 Rating:
|
1. Doubleclick on PID block 2. Select tab: I/O's 3. Select the parameters you wish to change 4. Scroll to the right to the tab: Unit 5. Select the unit of the parameter anda drop down menu appears 6. Select the desired unit 7. If you want units which aren't in the list like Nm3/h or uS then goto Plant view 8. Select "Shared declarations" , select "Units" and click on the right screen with right mouse to create a new unit. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
1 thankful Users |
Follow us on