(0)| 11/29/2022 7:41 AM | |
|
Joined: 5/6/2022 Last visit: 1/22/2026 Posts: 589 Rating:
|
Hellopaulohbsa__ at, As far as I understand, as I had the same question regarding the mirror function of an object, it is currently not possible in Unified and I hope that in future versions they will add this ability. But being able to rotate objects should be possible. I'm going to look into how to rotate objects. *Update* I found this way to rotate objects in the manual, in case it helps: "SIMATIC HMI WinCC Unified Engineering V17: Rotating an object around a pivot point" "SIMATIC HMI WinCC Unified Engineering V17: Rotating object” Best regards! |
Last edited by: ElonksuM_SN_BN at: 11/29/2022 07:50:19Last edited by: ElonksuM_SN_BN at: 11/29/2022 08:05:36If this Information really helps, you could use the Rate function |
|
| 3/25/2025 4:03 PM | |
|
Joined: 5/6/2019 Last visit: 1/22/2026 Posts: 2 Rating:
|
I used the Inkscape to solve this problem. 1. I have copied the ClassicPump.svghmi file located there: C:\Program Files\Siemens\Automation\Portal V19\Data\Hmi\SvgControls\IndustryGraphicLibrary\Pumps 2. Change the extention to .svg; 3. I opened the .svg file with Inkspace and used the mirror command there; 4. I saved the file under a different name; 5. I opened the file with Notepad++ and where it said ClassicPump I put the new name ClassicPulmpLeft, for example; 6. I changed the extension of the new file to .sgvhmi and copied the file to the location mentioned above; 7. Update the dynamic widgets on TIA Portal. AttachmentClassicPumpLeft.txt (167 Downloads) |
This contribution was helpful to
|
|
Follow us on