(0)| 7/8/2009 6:12 AM | |
|
Joined: 10/7/2005 Last visit: 1/21/2026 Posts: 3054 Rating:
|
Hello centers As per manual 30011 means: A function could not be executed because the function was assigned an invalid value or type in the parameter. The HMI system messages may contain parameters which are not decoded for the user but which are relevant in respect of the cause of an error since they provide a reference to the source code of the runtime software. These parameters are issued according to the text “Error code:”. |
|
Cheers |
|
Follow us on