4/4/2025 10:01 AM | |
Joined: 3/14/2008 Last visit: 9/8/2025 Posts: 2216 Rating:
|
Hi, Process tag types are the former CMT only they lack synchronization. With the PTT you can create a type and with the Import Export Assistent, you can create instances with some instance specific attributes you could configure. When instanced and you want to change some things, it's not always very easy to do so. It's a one way synchronization. The instances are linked to the Process Tag Type and deleting the connection will delete the PTT instance and set it back to a normal CFC. In order to be neo ready and make use of all the nice features PCS7 V9.0 and higher provides, I would suggest you use CMT's. In order to prevent extra work by creating newly CMT, you can migrate the PTT to CMT and create instances of the CMT which provides the use of variants, and much better synchronization. In order to make use of CMT and synchronization, you need an additional VXM license. The IEA is only needed if you want to create new instances of a PTT. |
If I could help you, you can use the RATE button. Thank you. |
|
4/30/2025 6:48 AM | |
Joined: 1/11/2019 Last visit: 8/14/2025 Posts: 899 Rating:
|
I request you to rise a service ticket for the same upgradation is involved |
Follow us on